Imagine a home HVAC running constantly, with no thermostat to control its operation relative to the interior temperature of the home. Seems wasteful and inefficient, right? A similar scenario can occur with smart-home devices and applications. If there’s not an intelligent manager of these devices, they can run all the time, wasting energy and money. In this article, learn about new Infineon XENSIV™ 60-GHz radar sensors and how their use in occupancy monitoring can lead to more efficient everyday life in a modern smart home.
The number of smart-home applications and connected devices is growing, making everyday life more convenient for their users. Yet this results in high energy consumption, as these devices are often permanently active or in standby mode in order to be ready for use at all times — even though no one is present. By equipping smart devices with the Infineon XENSIV™ 60-GHz radar sensor, they become more energy-efficient and therefore smarter and more sustainable.
Smart buildings and smart homes are becoming increasingly popular, and their number is expected to grow significantly in the coming years. Already today, the number of smart homes worldwide is estimated at more than 200 million, and forecasts predict that this figure will exceed 500 million within the next few years
(Figure 1).
A house can become smart only through increasingly digitalized devices with more and more ingenious functionalities. However, this comes at a high price: The need for energy is growing, despite the previous trend of steadily declining standby power consumption. Smart devices require energy even when they are “off,” as being in standby mode is the only way for them to react instantaneously to user input (e.g., via voice control) or to provide the latest information from the smart home or web. Furthermore, there are many occasions when it is completely unnecessary for a device to run in standby mode and thus consume energy — primarily when no one is present.
To solve this issue and to meet the requirements of both digitization and energy efficiency, Infineon leverages its semiconductor solutions. One of them is the XENSIV™ radar sensor, which can be applied to almost all smart-home devices. Radar sensors are highly sensitive and can detect whether a person is present and whether the device needs to be ready — similar to a screensaver that deactivates the PC monitor after a certain time without mouse or keyboard input and reactivates it as soon as new input is noticed. Through this reliable presence and absence detection, Infineon’s 60-GHz radar sensor powers the design of truly smart, energy-saving devices.
Activity Triggered By User Presence Versus Continuous Activity Or Standby
According to a Statista survey conducted in Germany in 2021 with 3,000 respondents aged 18 to 64 years, almost three-quarters own at least one smart-home device. In the U.S., the figures are similar (Figure 2), while in China, the percentage of users of smart-home devices is as high as 90%. The devices are as diverse as their applications: They include lighting; security devices; consumer electronics such as TVs, laptops, and soundbars; kitchen appliances; and air conditioners. But all these devices are increasing the demand for energy, which is an undesirable effect, especially in times of rising energy costs, when customers prefer energy-saving, sustainable, and eco-friendly devices. Moreover, the grid infrastructure is under increasing strain.
Instead of putting devices such as thermostats, smart speakers, and digital assistants into normal standby mode, one way to reduce energy consumption would be to put them into a “deep-sleep mode” when no one is present. For some devices, this can save a few watts or a fraction of that. But there are also use cases where you can save more than 100 W if you put devices into a deep sleep mode or temporarily switch them off whenever no one is present and they are therefore not needed — for example, the TV screen, the laptop, the sound system, and the air conditioner. By using a radar sensor, such devices will be able to sense the presence or movement of people; if these impulses remain absent, a radar-based smart device can automatically switch to sleep mode and save energy. Depending on the sensor and implementation, the radar module itself has a power consumption of only a few milliwatts and a maximum power consumption of 0.1 W, which is significantly lower than the energy demand of the “on” or standard standby mode of many electronic devices (Figure 3).
How To Use Radar Sensors To Increase Energy Efficiency
To save energy, the approach that devices must always be available and connected — this includes power-hungry standby mode — needs to be reinvented. We require devices that are only active or in standby when really necessary — in other words, when users are present. That is what we do today in our “nonsmart” homes, when we switch on the lights upon entering the room or manually activate the air conditioner only when it is getting too hot inside. Still, in many devices, power-saving features like timeout are not even implemented or are disabled by the user. This is often due to the fact that those features, in connection with high functionality, can lead to a long boot time and lack of up-to-date information, especially after inconvenient manual reactivation, so they would significantly worsen the customer experience.
But a new smart approach could be the answer to many questions: Why does the display of a thermostat always have to be on, and why does the device itself always have to be connected to the internet to download weather data? Why is the home security system’s camera always on, recording data, pre-processing it, and transferring it to the cloud, even though no one is moving in the area being monitored? The best way to accomplish a smarter way of activating devices is to implement motion detection enabled by a radar sensor to wake them from their deep-sleep mode.
For instance, the smart thermostat could be switched off by default while only a radar detection module is activated. As soon as the radar detects movement in the room, the thermostat would be activated to update the standard data from the house and the weather data from the internet. The display would turn on when someone enters a defined area, such as within a 1-meter radius of the device, so the user would not have to touch the screen to activate it and then wait for the data to be updated and the results to be displayed. This concept of presence detection can be deployed in many other smart-home devices and appliances.
Furthermore, the reverse principle of vacancy detection can also be applied, which offers an even bigger potential to save energy. In this case, devices such as televisions, loudspeakers, smart lamps, and air conditioners can be switched off if no movement is detected in the room for a certain period of time. This significantly reduces power consumption. Because vacancy detection is not about the immediate activation of a device, but the targeted deactivation when no one has been around for a while, the sensor module itself can remain deactivated and perform a check only every few seconds or minutes. As a result, such a sensor module can save a huge amount of energy for the whole system while consuming very little itself.
Buildings with HVAC systems especially can profit from this principle, as most energy is wasted for heating and cooling even though no one is present. To make matters worse, in many cases, these devices run frequently and for long periods. A truly smart home, however, would deactivate those systems as soon as the area has been vacated for a while. This feature is gradually becoming commonplace for lighting systems but not yet in air conditioners and other devices such as monitors, kitchen appliances, computers, speakers, and sound systems.
Users can also benefit from vacancy detection in other applications, such as televisions. For example, Infineon’s BGT60LTR11AIP radar sensor (Figure 4) has been implemented in Samsung’s Frame TV 2021 (Figure 5). The radar sensor switches the TV from Art Mode to Sleep Mode when nobody has been nearby for a user-specified time. This not only saves energy but also extends display lifetime.
Radar Sensors Are The Most Suitable Sensing Option For Smart-Home Devices
Of all the available motion-detection solutions, radar sensors have the highest sensitivity even for the smallest movements, some of which are even invisible to the human eye. PIR sensors cannot compete in terms of sensitivity. Also, radar does not rely on body heat as PIR sensors do, because it is an active sensing technology. This ensures that a person is detected even when they are barely moving or not moving at all. But arguably one of the biggest advantages is detection through non-conductive materials. While infrared, ultrasonic, camera, and other image-based sensors must not be covered or require openings in the product housing, a radar sensor can be completely hidden inside a device. As a result, you do not have to make any compromises in the design of the product and can avoid additional manufacturing steps and costs for a housing with corresponding adaptations.
Another possibility is camera-based motion detection — for example, for cameras, TVs, laptops, and other devices that already have a suitable image sensor. Image systems have very high power consumption, though they may need good ambient light conditions, and there is a need for image processing to detect motion from a video, which further requires a lot of energy. Lack of privacy is often also cited as a concern, as camera-based systems invade private spaces, so users do not fully trust them.
Furthermore, falling prices for consumer electronics are increasing cost pressure on components. Hence, 3D time-of-flight (ToF) and camera sensors are often too expensive to be implemented for presence detection. Even powerful PIR solutions, which not only affect the design of the product housing but also require an additional Fresnel lens, amplifier, controller, etc., increase the bill-of-materials cost. Infineon’s BGT60LTR11AIP radar sensor, by comparison, requires only a minimum of supporting components, especially in autonomous operation, and therefore has the smallest impact on system costs. Because of their tiny size, radar sensors can also be incorporated into small and thin electronic devices.
In addition, radar sensors are robust in dusty, smoky, or humid environments where some laser-based ToF sensors or other image-based sensors might be subject to deteriorations in their detection performance.
Additional Smart Functionalities Enabled By Radar Sensors
Poor handling of devices also leads to unnecessary power consumption. Users are not always aware of this, but they waste energy unintentionally when they fail to switch off their devices or adjust the settings when they are going to be temporarily absent. However, with the aid of radar sensors, this can be regulated automatically so that users don’t have to think about it but have the assurance that they are not wasting energy.
Besides being used as a presence or absence detector, radar sensors can add other functions to smart devices — for example, in air-conditioning systems. In such applications, radar sensors are most efficient when combined with temperature and CO2 sensors, so the system is activated as needed — for example, when someone is in the room, when the CO2 level is too high, or when the temperature exceeds the predefined limits. Whereas other sensing technologies often provide only binary information such as presence or absence, a radar sensor can also check the number of people in the room and adjust the level accordingly at an early stage, or even check the people’s positions and distances to control the direction of the airflow.
There are many other possible use cases — for example, sound systems that track the position of the listener and continuously optimize volume and sound parameters accordingly; TVs with child care, which measure the viewer’s distance and give a warning if the child’s eyes are too close to the screen; or devices for the elderly or people in need of care, such as alarm systems that call for assistance in the event of a fall. Thus, with little effort, radar sensors can save energy and contribute not only to people’s comfort but to their personal well-being and safety in a smart environment.
Download the original article here: