Explore how to find the right DC fan for your design in this article from Same Sky.
Same Sky's DC axial fans offer design flexibility in fan size, power consumption, noise, and more. With such an impressive variety of options, it’s important to think through a few critical elements before selecting the right DC fan for your design. This includes calculating the airflow and air pressure of your design, understanding the airflow requirements within a fan’s operating curve, considering whether or not to run multiple fans in parallel or in a series, and the overall effects of a fan’s speed on your design. Learn more about these considerations and get a better understanding on how to find the right DC fan for your design with this article from Same Sky.
Important airflow parameters
Before a fan can be specified for a particular system, there are a few parameters that are important to understand regarding airflow and heat transfer. Moving air is effective in cooling objects by absorbing heat from the object and then transferring that heat elsewhere to be dissipated. The amount of energy transferred is dependent upon the mass of the moving air, the specific heat of the moving air, and the temperature change imparted to the moving air.
The mass of the moving air can be calculated from the volume of air being moved and the density of the moving air.
Substituting the second equation into the first relates the energy dissipated to the volume of air involved.
Dividing both sides of the equation by time produces the following form of the equation.
In most applications the excess power (inefficiency of the system) is known and the airflow (volume/time) is unknown. Thus, the equation can be arranged as shown below.
As discussed in our previous blog post, this equation is commonly written as:
Where
Q = airflow
q = heat to be dissipated
ρ = density of the air
Cp = specific heat of the air
ΔT = the temperature the air will rise when absorbing the heat to be dissipated
k = a constant value, dependent upon the units used in the other parameters
The density of dry air at sea level at 68°F (20°C) is 0.075 lbs/ft3 (1.20 kg/m3) and the specific heat of dry air is 0.24 Btu/lb °F (1 kJ/kg °C). Using these values for density and specific heat the above equation simplifies to:
Qf = 1.8q/ΔTC
Qm = 0.09q/ΔTF
Qm = 0.05q/ΔTC
Where
Qf = airflow in Cubic Feet per Minute (CFM)
Qm = airflow in Cubic Meters per Minute (CMM)
q = heat to be dissipated in Watts
ΔTF = the temperature the air will rise when absorbing the heat to be dissipated in °F
ΔTC = the temperature the air will rise when absorbing the heat to be dissipated in °C
Air pressure
The above equations state the airflow rate required to cool a product. It is also necessary to know the pressure at which the airflow is to be delivered by the fan. The path of the airflow through the product to be cooled will create a resistance to the flow of the air. Fans should be selected to produce sufficient pressure to force the required volume of air through the product to enable the desired cooling. Calculating the required pressure will be a separate task for each unique product and cannot be simplified in a manner similar to the flow rate calculations. Many CAD products are available to calculate the air pressure and airflow characteristics of a design, while anemometers and manometers can be used to measure the air speed and pressure characteristics once a design is completed.

Figure 1: Characterizing and plotting airflow versus pressure
Achieving required airflow and pressure
Based upon concepts from the previous two sections, an airflow rate and air pressure must be created by the fan (or fans) to provide the required cooling. Datasheets from fan manufactures will provide a value of airflow rate with no back pressure, a value of maximum pressure with no airflow rate, and a curve of the airflow versus the pressure available from the fan. Take for example a product whose airflow requirements have been calculated to be 10 CFM or greater based upon the heat to be removed and the air temperature limits. The mechanical design of the product has been characterized to produce the airflow versus pressure graph shown in Figure 2. The dashed line denotes the minimum airflow required for the product (greater airflow is also acceptable), while the orange curve represents the relationship between pressure and airflow for the mechanical design of the product.

Figure 2: System requirements, airflow versus static pressure
Based upon the curves in Figure 2, Same Sky's CFM-6025V-131-167 dc axial fan has been selected for the project. The datasheet for the dc fan specifies 16 CFM of airflow with no back pressure, static pressure of 0.1 inH2O with no airflow, and also provides the graph in Figure 3.

Figure 3: Same Sky's CFM-6025V-131-167 performance graph
Overlaying the system requirements from Figure 2 on the dc fan characteristics from Figure 3 produces the graph in Figure 4.

Figure 4: System requirements and fan performance
The operating point highlighted by the red circle in figure 4 indicates the pressure and airflow for the system with the selected fan. It should be noted that the airflow requirement was calculated to be 10 CFM and the fan will provide 11.5 CFM of airflow. For some applications this will be a sufficient thermal operating margin, while in other applications this solution may not provide enough margin.
Operating fans in parallel or series
In general, larger or faster fans will provide greater maximum airflow and greater maximum pressure. If a single fan is unable to deliver the required airflow or pressure, then two or more fans can be operated physically in parallel or in series. Operating fans in parallel will increase the maximum available airflow, but will not increase the maximum pressure, whereas operating fans in series will increase the maximum available pressure, but will not increase the maximum available airflow.

Figure 5: Operating multiple fans in series or in parallel
The performance curve for operating multiple fans in parallel can be easily generated by the user. The combined fan airflow versus pressure curve for multiple fans operated in parallel is identical to the single fan graph, with the only change being the values of airflow are multiplied by the number of fans operated in parallel.

Figure 6: Operating fans in parallel multiplies airflow by number of fans
The performance curve for operating multiple fans in series can be generated in a similar manner, with the pressure values altered by the number of fans in series. Ultimately, multiple fans in parallel provide the greatest improvement for high airflow and low-pressure systems, while multiple fans in series provide the greatest improvement for high pressure and low airflow systems.

Figure 7: Multiple fans in high and low airflow resistance systems
Effects of fan speed
The speed of the fan (RPM) can be determined by the initial selection of the fan or by a fan control signal. Changing the speed of the fan will affect the air volume, the air pressure, the power consumed, and the acoustic noise produced by the fan. These relationships are described by what are called the "fan affinity laws".
Fan affinity laws
The volume of air moved by the fan is proportional to the speed of the fan.
- CFM α RPM
- i.e. 3 x RPM produces 3 x CFM
The pressure of air from the fan is proportional to the square of the speed of the fan.
- Air pressure α RPM2
- i.e. 3 x RPM produces 9 x pressure
The power required to operate a fan increases by the cube of the speed of the fan.
- Power α RPM3
- i.e. 3 x RPM requires 27 x power
The acoustic noise produced by a fan will increase by 15 dB when the speed of the fan is doubled.
- A 10 dB increase in acoustic noise is typically perceived by human hearing as a doubling of the noise level

Figure 8: Fan affinity laws graph
Conclusion
With knowledge of the required airflow and pressure, the proper fan (or fans) can be selected to provide adequate cooling. Operating fans in parallel or in series provides designers with additional options to meet the thermal requirements of their application when a single fan may not be sufficient. Same Sky's line of dc axial fans features a variety of performance ratings, allowing designers flexibility when choosing between fan size, power consumed, audible noise produced, and more.